S32 Flash Tool failed in S32G-VNP-RDB3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Flash Tool failed in S32G-VNP-RDB3

ソリューションへジャンプ
2,088件の閲覧回数
neilpatrick32
Contributor I

Hi NXP Community,

I am using the S32G-VNP-RDB3 evaluation board (S32G399A).

According to "UGS32G-VNP-RDB3" I configured the DIP Switches following the "3.2 Default Switch Setting" setting, but also change for the "3.7 Switch Setting for Serial Boot"

3.2 Default Switch Setting.JPG

3.7 Switch Setting for Serial Boot.JPG

Settings for the UART COM which is connected to UART0.

UART settings.JPG

Then i followed the procedure from "AN13727", but i got this error always.

S32 Flash tool.JPG

The light from the UART0 is visible whenever uploading to the target.

Could you please support me? Thanks!

1 解決策
2,062件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have seen that there is a ticket under the ticket support, which we have answered to it.

Still, we seem to have missed some information. We have our COM set with the following properties:

DanielAguirre_0-1691174353307.png

If you set your COM with 9600 baudrate does it happen the same? If you like to continue your support on the NXP support case we do not have any problem.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,063件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have seen that there is a ticket under the ticket support, which we have answered to it.

Still, we seem to have missed some information. We have our COM set with the following properties:

DanielAguirre_0-1691174353307.png

If you set your COM with 9600 baudrate does it happen the same? If you like to continue your support on the NXP support case we do not have any problem.

Please, let us know.

0 件の賞賛
返信