Path Not Found Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
9,239件の閲覧回数
shyamsundar121
Contributor II

Hello 

I have created a new workspace and imported project. This code doesn't have any errors but it has path error as listed below. Please help me to resolve the issue.

Description Resource Path Location Type
Ld error: Cannot run program "": Launching failed C/C++ Problem

Description Resource Path Location Type
Program "" not found in PATH _2W_60V_NXP_ADI_IIT C/C++ Problem

Description Resource Path Location Type
Program "C:\NXP\S32DS_ARM_v2018.R1\Cross_Tools\gcc-arm-none-eabi-4_9\bin\arm-none-eabi-" not found in PATH _2W_60V_NXP_ADI_IIT Project Properties, C++ Preprocessor Include.../Providers, [CDT S32DS Built-in Compiler Settings] options C/C++ Scanner Discovery Problem

Description Resource Path Location Type
SDK Id=S32K144_SDK_3.0.0_PATH for the Project "_2W_60V_NXP_ADI_IIT" is not found in SDKs list! Ignored. _2W_60V_NXP_ADI_IIT P/_2W_60V_NXP_ADI_IIT Missed SDK Marker

Description Resource Path Location Type
SDK Id=S32K14x_AMMCLIB_gcc_1.1.18_PATH for the Project "_2W_60V_NXP_ADI_IIT" is not found in SDKs list! Ignored. _2W_60V_NXP_ADI_IIT P/_2W_60V_NXP_ADI_IIT Missed SDK Marker

shyamsundar121_0-1651056103396.pngshyamsundar121_0-1651056103396.png

Thanks and regards

Shyam Sundar

0 件の賞賛
返信
1 解決策
9,116件の閲覧回数
shyamsundar121
Contributor II

I found this error is due to importing of projects from older version to newer version. It is creating sdk mismatch so triggering sdk missing error. I have started working with older version. Please let me know if you can resolve

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
8,324件の閲覧回数
RachelGomez123
Contributor I

Tips to fix-

Double-Check the Path Names. 
Temporarily Disable Your Antivirus. 
Try to Connect Using an IP Address. 
Restart the TCP/IP NetBIOS Helper Service.

Regards,

Rachel Gomez

0 件の賞賛
返信
8,462件の閲覧回数
RachelGomez123
Contributor I

Solution 1: Check path for errors.
Solution 2: Check directory or folder.
Solution 3: Remove invalid environment variable.
Solution 4: Repair system files with SFC and DISM.
Solution 5: Clean up Windows update.
Solution 6: Reset Windows update components.

 

Regards,

Rachel Gomez

0 件の賞賛
返信
9,117件の閲覧回数
shyamsundar121
Contributor II

I found this error is due to importing of projects from older version to newer version. It is creating sdk mismatch so triggering sdk missing error. I have started working with older version. Please let me know if you can resolve

0 件の賞賛
返信
9,103件の閲覧回数
Andy_Pu
Contributor I

Hi Shyam Sundar,

     Thank you!Following your reply,I borrowed my colleague's computer to load the project then the problem solved.I never thought of this!

Andy

0 件の賞賛
返信
9,127件の閲覧回数
Andy_Pu
Contributor I

I am facing the same problem,have you find a solution yet?I'll be appreciate if you can tell me.

0 件の賞賛
返信