PWM capture in S32G linux bsp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM capture in S32G linux bsp

2,689 Views
xiaochun
Contributor I

Hello NXP,

These days I try to use PWM capture function of S32G3. PWM output is OK. But PWM capture doesn't work.

root@ubuntu-s32g399ardb3:/sys/devices/platform/soc/402e4000.pwm/pwm/pwmchip6/pwm0# cat capture
cat: capture: Function not implemented

So, How can I use pwm capture in linux application? thanks!

 

0 Kudos
Reply
4 Replies

2,670 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which BSP version are you using?

Please, let us know.

0 Kudos
Reply

2,668 Views
xiaochun
Contributor I

Hello Daniel-Aguirre,

The used BSP version is Linux BSP 33.0.

Thanks!

0 Kudos
Reply

2,613 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

We do apologize for the delay.

We have the following update from our internal team:

"The PWM capture feature is not supported at this moment. I also didn't find any plan to implement this feature in S32G software offering schedule.

However, the S32G FlexTimer(FTM) support pin input capture (on rising edges, falling edges or both edges), customers could implement this feature through their own code."

Please, let us know.

0 Kudos
Reply

2,656 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

It may seem that the driver being used might not have the capture function integrated into it.

Let us confirm this situation with our internal team.

Please, let us know.

0 Kudos
Reply