PWM capture in S32G linux bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM capture in S32G linux bsp

2,718件の閲覧回数
xiaochun
Contributor I

Hello NXP,

These days I try to use PWM capture function of S32G3. PWM output is OK. But PWM capture doesn't work.

root@ubuntu-s32g399ardb3:/sys/devices/platform/soc/402e4000.pwm/pwm/pwmchip6/pwm0# cat capture
cat: capture: Function not implemented

So, How can I use pwm capture in linux application? thanks!

 

0 件の賞賛
返信
4 返答(返信)

2,699件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which BSP version are you using?

Please, let us know.

0 件の賞賛
返信

2,697件の閲覧回数
xiaochun
Contributor I

Hello Daniel-Aguirre,

The used BSP version is Linux BSP 33.0.

Thanks!

0 件の賞賛
返信

2,642件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

We do apologize for the delay.

We have the following update from our internal team:

"The PWM capture feature is not supported at this moment. I also didn't find any plan to implement this feature in S32G software offering schedule.

However, the S32G FlexTimer(FTM) support pin input capture (on rising edges, falling edges or both edges), customers could implement this feature through their own code."

Please, let us know.

0 件の賞賛
返信

2,685件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

It may seem that the driver being used might not have the capture function integrated into it.

Let us confirm this situation with our internal team.

Please, let us know.

0 件の賞賛
返信