PFE UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,149 次查看
sophie-wang
Contributor III

Hi NXP Expert,

I found PFE_UART in S32G2_Schematic_Checklist.xlsx,Please kindly check picture below.Would you please help to check what is it. My customer need 8 uart ports. We can found 3 FlexD uart and 4LLCE LIN. What should they do if they need one more uart com port?

Thank you

Sophie

0 项奖励
回复
1 解答
1,138 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The PFE_UART_RX/TX signals are for NXP internal use only, they are not for general application use.

As for more UART ports, as you are saying, 7 UART ports is the limit for the S32G2. If you are looking to add more ports, there are available chips that could be connected externally to the S32G to add more serial ports. It just depends on the general implementation you are trying to achieve.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,139 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The PFE_UART_RX/TX signals are for NXP internal use only, they are not for general application use.

As for more UART ports, as you are saying, 7 UART ports is the limit for the S32G2. If you are looking to add more ports, there are available chips that could be connected externally to the S32G to add more serial ports. It just depends on the general implementation you are trying to achieve.

Please, let us know.

0 项奖励
回复