PFE UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,030件の閲覧回数
sophie-wang
Contributor III

Hi NXP Expert,

I found PFE_UART in S32G2_Schematic_Checklist.xlsx,Please kindly check picture below.Would you please help to check what is it. My customer need 8 uart ports. We can found 3 FlexD uart and 4LLCE LIN. What should they do if they need one more uart com port?

Thank you

Sophie

0 件の賞賛
返信
1 解決策
2,019件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The PFE_UART_RX/TX signals are for NXP internal use only, they are not for general application use.

As for more UART ports, as you are saying, 7 UART ports is the limit for the S32G2. If you are looking to add more ports, there are available chips that could be connected externally to the S32G to add more serial ports. It just depends on the general implementation you are trying to achieve.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,020件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The PFE_UART_RX/TX signals are for NXP internal use only, they are not for general application use.

As for more UART ports, as you are saying, 7 UART ports is the limit for the S32G2. If you are looking to add more ports, there are available chips that could be connected externally to the S32G to add more serial ports. It just depends on the general implementation you are trying to achieve.

Please, let us know.

0 件の賞賛
返信