How to install S32G2 RTD drivers and Platform Software integration releases in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to install S32G2 RTD drivers and Platform Software integration releases in S32DS

ソリューションへジャンプ
3,401件の閲覧回数
zhuliya
Contributor I

I got two package as :

SW32G2_RTD_4.4_2.0.0_P03_D2109.exe

Platform_Software_Integration_S32G2XX_2021_07_01.exe.

But I don't know how to install them in S32DS.

Could you please help? Thank you.

"Make sure the required RTD drivers (as per Software prerequisites chapter) and Platform
Software integration releases are installed in S32DS by using the update site archives from
the release package"

0 件の賞賛
返信
1 解決策
3,394件の閲覧回数
bpe
NXP Employee
NXP Employee

The package you downloaded are standalone. You cannot install them into S32DS.

Platform Software Integration examples are available standalone only. Run
the .exe file on a Windows PC to install them. Note that the release you
obtained depends on RTD 2.0.0 HF2, not P03. Install the verified version to
avoid problems.

To install RTD as an S32DS plugin, download the file that has the .zip extension
and follow the instructions in the package Release Notes.

Hope this helps,
Platon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,395件の閲覧回数
bpe
NXP Employee
NXP Employee

The package you downloaded are standalone. You cannot install them into S32DS.

Platform Software Integration examples are available standalone only. Run
the .exe file on a Windows PC to install them. Note that the release you
obtained depends on RTD 2.0.0 HF2, not P03. Install the verified version to
avoid problems.

To install RTD as an S32DS plugin, download the file that has the .zip extension
and follow the instructions in the package Release Notes.

Hope this helps,
Platon

0 件の賞賛
返信