How to install S32G2 RTD drivers and Platform Software integration releases in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install S32G2 RTD drivers and Platform Software integration releases in S32DS

Jump to solution
2,014 Views
zhuliya
Contributor I

I got two package as :

SW32G2_RTD_4.4_2.0.0_P03_D2109.exe

Platform_Software_Integration_S32G2XX_2021_07_01.exe.

But I don't know how to install them in S32DS.

Could you please help? Thank you.

"Make sure the required RTD drivers (as per Software prerequisites chapter) and Platform
Software integration releases are installed in S32DS by using the update site archives from
the release package"

0 Kudos
Reply
1 Solution
2,007 Views
bpe
NXP Employee
NXP Employee

The package you downloaded are standalone. You cannot install them into S32DS.

Platform Software Integration examples are available standalone only. Run
the .exe file on a Windows PC to install them. Note that the release you
obtained depends on RTD 2.0.0 HF2, not P03. Install the verified version to
avoid problems.

To install RTD as an S32DS plugin, download the file that has the .zip extension
and follow the instructions in the package Release Notes.

Hope this helps,
Platon

View solution in original post

0 Kudos
Reply
1 Reply
2,008 Views
bpe
NXP Employee
NXP Employee

The package you downloaded are standalone. You cannot install them into S32DS.

Platform Software Integration examples are available standalone only. Run
the .exe file on a Windows PC to install them. Note that the release you
obtained depends on RTD 2.0.0 HF2, not P03. Install the verified version to
avoid problems.

To install RTD as an S32DS plugin, download the file that has the .zip extension
and follow the instructions in the package Release Notes.

Hope this helps,
Platon

0 Kudos
Reply