How to activate TJA1153 PHY on RDB2/GoldBox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to activate TJA1153 PHY on RDB2/GoldBox

ソリューションへジャンプ
7,680件の閲覧回数
JetXiong
NXP Employee
NXP Employee

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN.

NOTE:
Only the boards with series number listed in attached spreadsheet need this activation. The serial number of your boards can be found on the label on the back of your boards. Refer to the following guide for more information. 

Jet
0 件の賞賛
返信
1 解決策
7,579件の閲覧回数
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi, 

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN. Refer to the guide for detail information.

Best Regards,

Frank

元の投稿で解決策を見る

3 返答(返信)
7,580件の閲覧回数
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi, 

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN. Refer to the guide for detail information.

Best Regards,

Frank

6,576件の閲覧回数
frank_fr_lin
Contributor I

Hi NXP ,

Is there a TJA1153_Local_Activation(RDB2) S32DS Project file available for download?

Thanks

0 件の賞賛
返信
7,662件の閲覧回数
bpe
NXP Employee
NXP Employee

If you wish to receive suggestions, please provide a meaningful problem description.

Best Regards,
Platon

0 件の賞賛
返信