How to activate TJA1153 PHY on RDB2/GoldBox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to activate TJA1153 PHY on RDB2/GoldBox

Jump to solution
7,706 Views
JetXiong
NXP Employee
NXP Employee

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN.

NOTE:
Only the boards with series number listed in attached spreadsheet need this activation. The serial number of your boards can be found on the label on the back of your boards. Refer to the following guide for more information. 

Jet
0 Kudos
Reply
1 Solution
7,605 Views
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi, 

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN. Refer to the guide for detail information.

Best Regards,

Frank

View solution in original post

3 Replies
7,606 Views
Frank_Jianpeng_Zhao
NXP Employee
NXP Employee

Hi, 

This guide provides a simple method to activate the TJA1153 on the S32G-VNP-RDB2/GoldBox for enabling CAN communication. After this activation of the TJA1153 by following steps, it will operate as a CAN PHY. Contact NXP for further details about Secure CAN Transceiver or visit http://www.nxp.com/CAN. Refer to the guide for detail information.

Best Regards,

Frank

6,602 Views
frank_fr_lin
Contributor I

Hi NXP ,

Is there a TJA1153_Local_Activation(RDB2) S32DS Project file available for download?

Thanks

0 Kudos
Reply
7,688 Views
bpe
NXP Employee
NXP Employee

If you wish to receive suggestions, please provide a meaningful problem description.

Best Regards,
Platon

0 Kudos
Reply