GDB debug with s32g2 in linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GDB debug with s32g2 in linux

1,277 次查看
0xEC
Contributor IV

hi everyone,

i have been trying to develop yocto linux in s32g274a series SoC. I need to debug ATF, U-Boot and Image itself. I have s32 debug probe and my development environment is Ubuntu 22.04, current version of S32DS is not supported in Ubuntu 22.04. Can i debug my target by using S32 Debug Probe by using gdb, i need to connect target via debugger but i could not find any executable which connect to s32 debugger in server mode.

best,

标记 (2)
0 项奖励
回复
2 回复数

1,242 次查看
nxf92355
NXP Employee
NXP Employee

Hi Erhan

 

Hope you are doing well

I think s32ds is required for same .i will ask to our internal team for clarification and will update here as soon as i got any update

Regards ,

Tushar

 

 

1,157 次查看
nxf92355
NXP Employee
NXP Employee

Hi Erhan

 

Sorry for late reply as i was on leave. S32DS is required for same , you can refer follow link. we recommend to use ubuntu 18.04  or 20.04 for s32ds

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Command-Line-GDB-Debugging-with-...

let us know if any more quarry

 

Regards ,

Tushar

 

0 项奖励
回复