ATF Build Parameters-FIP_QSPI_OFFSET

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ATF Build Parameters-FIP_QSPI_OFFSET

ソリューションへジャンプ
3,914件の閲覧回数
Coco111
Contributor III

My NXP friends:

              In the ATF source code, I couldn't find any information about make FIP_ QSPI_ OFFSET, FIP_ MMC_ OFFSET, FIP_ MEMORY_ OFFSET, Can you tell me why? Thank you.

 

Screenshot from 2023-05-18 22-14-43.pngScreenshot from 2023-05-18 22-14-43.pngScreenshot from 2023-05-18 22-16-20.pngScreenshot from 2023-05-18 22-16-20.png

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
3,867件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. As said in the BSP Reference Manual:

"For QSPI boot, configure TF-A to read the FIP image from a defined QSPI offset."

"For SD/eMMC boot, configure TF-A to read the FIP image from a defined SD/eMMC offset."

"Configure TF-A to read the FIP image from a defined memory address instead of reading it from the boot source storage (QSPI or MMC)."

These options should let you have control over where you want the ATF to be looking for the FIP image, depending on which interface you want to search over (QSPI, MMC or SRAM).

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,896件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are not understanding the overall request. We do apologize.

What information are you looking for on regards of "FIP_ QSPI_ OFFSET, FIP_ MMC_ OFFSET, FIP_ MEMORY_ OFFSET"?

We do see they are used under the file you are referring to.

Please, let us know.

0 件の賞賛
返信
3,887件の閲覧回数
Coco111
Contributor III
I have read the Linux BSP user manual and do not quite understand the functions of these three macros. Therefore, I looked at the specific code in the ATF source code, but I found that there is no corresponding C code to handle these three macros
0 件の賞賛
返信
3,868件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. As said in the BSP Reference Manual:

"For QSPI boot, configure TF-A to read the FIP image from a defined QSPI offset."

"For SD/eMMC boot, configure TF-A to read the FIP image from a defined SD/eMMC offset."

"Configure TF-A to read the FIP image from a defined memory address instead of reading it from the boot source storage (QSPI or MMC)."

These options should let you have control over where you want the ATF to be looking for the FIP image, depending on which interface you want to search over (QSPI, MMC or SRAM).

Please, let us know.

0 件の賞賛
返信
3,848件の閲覧回数
Coco111
Contributor III

Thank you for your reply. I understand
0 件の賞賛
返信