A core kernel panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A core kernel panic

2,648件の閲覧回数
Abhiram_m_s
Contributor I

Hello,

When we start both m core and a core together,  we are facing kernel panic issue in A core side and some of the features like CAN and I2C are not working in m core side.
What might be the issue

Here is the error message

Abhiram_m_s_0-1718370266670.pngAbhiram_m_s_0-1718370266670.png

I have attached the kernel log file. 

 

0 件の賞賛
返信
2 返答(返信)

2,607件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This is a problem of the kernel itself don't find memory to execute, check your ddr, do a  ddr stress memory and/or build the kernel again.

Regards

0 件の賞賛
返信

2,564件の閲覧回数
Abhiram_m_s
Contributor I

Hello,
When we remove llce and pfe distro feature, then it is booting properly. We feel the issue is due to resource conflicts between M and A core. Can you please let me know how to configure llce as slave so that it can boot properly.

0 件の賞賛
返信