processor expert generated empty files in S32DS PA V2.1 SDK 3.0.0 example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

processor expert generated empty files in S32DS PA V2.1 SDK 3.0.0 example

1,171 次查看
bingwang312
Contributor III

I just started to learn examples of SDK 3.0.0 on my devkit MPC5744P, so far i have not got any example working.  an interesting error is, i configured exponents everything, then clicked to processor expert to generate codes, at the first time when i checked some missing .h/.c header files, the folder and files were not there , the second time when i checked then, the folder and files automatically been created, confussing thing is these files are empty. i deleted those empty files, copied same files from another project, then generate code with PE again, these files became empty again. see the pictures below, any suggestion?

bingwang312_0-1639367132318.pngbingwang312_1-1639367168095.pngbingwang312_2-1639367185609.pngbingwang312_3-1639367197192.png

 

标签 (1)
0 项奖励
回复
0 回复数