Why do the examples from the same SDK generate the files of different names

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why do the examples from the same SDK generate the files of different names

ソリューションへジャンプ
1,496件の閲覧回数
jetty1012
Contributor II

I'm using S32DS v3.5, SDK v2.0.1

When I'm using I2c_IP_LPI2C_Transfer_S32K312_example, it generates the driver code with the name xx_VS_0_PBcfg.c (Right side)

And when I'm using another example or a new project, it generate the driver code with the name xx_BOARD_Init_Peripherals_PBcfg.c (Left side)

The configurations are the same, but why they generate the files of different names?

jetty1012_0-1685585957038.jpeg

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,487件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,488件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,475件の閲覧回数
jetty1012
Contributor II
So it's just file names that are different?
It doesn't affect the functions, yes?
0 件の賞賛
返信
1,469件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

It doesn't affect the functions. The name is up to you.

0 件の賞賛
返信