Why do the examples from the same SDK generate the files of different names

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why do the examples from the same SDK generate the files of different names

Jump to solution
1,573 Views
jetty1012
Contributor II

I'm using S32DS v3.5, SDK v2.0.1

When I'm using I2c_IP_LPI2C_Transfer_S32K312_example, it generates the driver code with the name xx_VS_0_PBcfg.c (Right side)

And when I'm using another example or a new project, it generate the driver code with the name xx_BOARD_Init_Peripherals_PBcfg.c (Left side)

The configurations are the same, but why they generate the files of different names?

jetty1012_0-1685585957038.jpeg

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,564 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,565 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,552 Views
jetty1012
Contributor II
So it's just file names that are different?
It doesn't affect the functions, yes?
0 Kudos
Reply
1,546 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

It doesn't affect the functions. The name is up to you.

0 Kudos
Reply