Why do the examples from the same SDK generate the files of different names

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why do the examples from the same SDK generate the files of different names

跳至解决方案
1,503 次查看
jetty1012
Contributor II

I'm using S32DS v3.5, SDK v2.0.1

When I'm using I2c_IP_LPI2C_Transfer_S32K312_example, it generates the driver code with the name xx_VS_0_PBcfg.c (Right side)

And when I'm using another example or a new project, it generate the driver code with the name xx_BOARD_Init_Peripherals_PBcfg.c (Left side)

The configurations are the same, but why they generate the files of different names?

jetty1012_0-1685585957038.jpeg

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,494 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,495 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

You can change the Name in Functional groups:

Functional groups Name.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,482 次查看
jetty1012
Contributor II
So it's just file names that are different?
It doesn't affect the functions, yes?
0 项奖励
回复
1,476 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

It doesn't affect the functions. The name is up to you.

0 项奖励
回复