Type writing to APSR without specifying a bitmask is deprecated.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Type writing to APSR without specifying a bitmask is deprecated.

4,101 Views
liufei
Contributor III

I'm starting with S32DS for paltform and I've found a problem after build project. 

The error is at c:\Users\LIU-FE~1\AppData\Local\Temp\ccGz3VHQ.s, in line 123, and have a error message "Type writing to APSR without specifying a bitmask is deprecated".

I've attached Problem screenshot. Can someone help me?

0 Kudos
Reply
6 Replies

4,034 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @liufei,

I would suggest that you can create a ticket in our NXP support portal: support.nxp.com, and after that please share your S32DS project so that we can check.

Best Regards,
Nam

0 Kudos
Reply

4,032 Views
liufei
Contributor III

Hello Nam,

Thanks for the reply,I'm sorry I can not share my project because confidential,but I can create a ticket in  NXP support portal: support.nxp.com,

So,it can be resolved without project?

 

BestRegards,

Liufei

0 Kudos
Reply

4,029 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @liufei,

It could be. Please create a ticket in NXP support portal.

Thank you,

Nam

0 Kudos
Reply

4,087 Views
mikedoidge
NXP Employee
NXP Employee

Hello @liufei,

I can see from the image that you are working with S32K1xx family device. Which specific device is it?

You indicate you are using S32DS, but is it S32 Design Studio for Arm or S32 Design Studio for S32 Platform? And which release version?

Are you using the S32 SDK or RTD?

What toolchain are you using? GCC?

Please provide more details.

Best Regards,

Mike

0 Kudos
Reply

4,074 Views
liufei
Contributor III

Hello Mark,

>I can see from the image that you are working with S32K1xx family device. Which specific device is it?

S32K148 with 144pin.

>but is it S32 Design Studio for Arm or S32 Design Studio for S32 Platform? And which release version?

S32 Design Studio for S32 Platform

>Are you using the S32 SDK or RTD?

Not using the SDK,I using MCAL(S32K1XX_MCAL4_2_RTM_1_0_5_D220111.exe)

>What toolchain are you using? GCC?

GCC V9.2

 

Best Regards,

Liu

 

0 Kudos
Reply

4,046 Views
mikedoidge
NXP Employee
NXP Employee

Hi @namnguyenviet,

It seems this is an MCAL issue, could you please help?

Thanks,

Mike

0 Kudos
Reply