Type writing to APSR without specifying a bitmask is deprecated.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Type writing to APSR without specifying a bitmask is deprecated.

4,047 次查看
liufei
Contributor III

I'm starting with S32DS for paltform and I've found a problem after build project. 

The error is at c:\Users\LIU-FE~1\AppData\Local\Temp\ccGz3VHQ.s, in line 123, and have a error message "Type writing to APSR without specifying a bitmask is deprecated".

I've attached Problem screenshot. Can someone help me?

0 项奖励
回复
6 回复数

3,980 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello @liufei,

I would suggest that you can create a ticket in our NXP support portal: support.nxp.com, and after that please share your S32DS project so that we can check.

Best Regards,
Nam

0 项奖励
回复

3,978 次查看
liufei
Contributor III

Hello Nam,

Thanks for the reply,I'm sorry I can not share my project because confidential,but I can create a ticket in  NXP support portal: support.nxp.com,

So,it can be resolved without project?

 

BestRegards,

Liufei

0 项奖励
回复

3,975 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello @liufei,

It could be. Please create a ticket in NXP support portal.

Thank you,

Nam

0 项奖励
回复

4,033 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @liufei,

I can see from the image that you are working with S32K1xx family device. Which specific device is it?

You indicate you are using S32DS, but is it S32 Design Studio for Arm or S32 Design Studio for S32 Platform? And which release version?

Are you using the S32 SDK or RTD?

What toolchain are you using? GCC?

Please provide more details.

Best Regards,

Mike

0 项奖励
回复

4,020 次查看
liufei
Contributor III

Hello Mark,

>I can see from the image that you are working with S32K1xx family device. Which specific device is it?

S32K148 with 144pin.

>but is it S32 Design Studio for Arm or S32 Design Studio for S32 Platform? And which release version?

S32 Design Studio for S32 Platform

>Are you using the S32 SDK or RTD?

Not using the SDK,I using MCAL(S32K1XX_MCAL4_2_RTM_1_0_5_D220111.exe)

>What toolchain are you using? GCC?

GCC V9.2

 

Best Regards,

Liu

 

0 项奖励
回复

3,992 次查看
mikedoidge
NXP Employee
NXP Employee

Hi @namnguyenviet,

It seems this is an MCAL issue, could you please help?

Thanks,

Mike

0 项奖励
回复