Hello Mark,
>I can see from the image that you are working with S32K1xx family device. Which specific device is it?
S32K148 with 144pin.
>but is it S32 Design Studio for Arm or S32 Design Studio for S32 Platform? And which release version?
S32 Design Studio for S32 Platform
>Are you using the S32 SDK or RTD?
Not using the SDK,I using MCAL(S32K1XX_MCAL4_2_RTM_1_0_5_D220111.exe)
>What toolchain are you using? GCC?
GCC V9.2
Best Regards,
Liu