The Flash Programmer feature in S32DS is not available.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Flash Programmer feature in S32DS is not available.

ソリューションへジャンプ
3,164件の閲覧回数
johns_chuang
Contributor III

Dear Team,

How should I configure the "Flash Programmer" in S32DS to use it? My S32DS can use the Debug function to flash the program to the MCU, but the "Flash Programmer" button in the UI is grayed out and cannot be used. How can I configure it to be functional?

FlashUp.JPG

S32 Design Studio for S32 Platform

Version: 3.6.0

Build id: 241128

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,912件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

PEMicro is responsible for their scripts and SW for programming/debugging. Other than the S32DS IDE debug scripts, I am not familiar with other alternatives.

Debuggers such as J-Link (SEGGER) provides the J-FLASH software which is free of charge.

Best regards,
Julián

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,147件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

S32 Flash Tool does not completely support S32K3 family yet. You can find the supported devices under C:\NXP\S32DS.3.6.0\S32DS\tools\S32FlashTool\doc\S32_Flash_Tool_Release_Notes.pdf

1.2. Supported devices
Flash Tool provides support for the following NXP devices:
• S32R41
• S32R45
• S32G2xx
• S32G3xx
• S32Z2/E2

Best regards,
Julián

0 件の賞賛
返信
3,132件の閲覧回数
johns_chuang
Contributor III

Hi Julián,

May I ask if there are any other methods or user interfaces available to program the S32K3xx, aside from just using Debug?

Thank you for your assistance.

Best,

Johns

0 件の賞賛
返信
3,107件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

If you are using an external debugger, you can use a flashing script instead of the Debug. For example, Lauterbach debugger comes with flashing script when installed: Lauterbach SW Flashing script(.Cmm) for the NXP-S32K322 Micro - NXP Community.

Best regards,
Julián

 

0 件の賞賛
返信
2,950件の閲覧回数
johns_chuang
Contributor III

Hi Julián,

We are using the Universal Multilink recommended on the S32K3 website, but when I inquired with PEmicro, they only offer the paid PROGACMP.

Do you know of any free programming software that can be used with Universal Multilink?

Thank you for your help.

Best,

Johns

タグ(1)
0 件の賞賛
返信
2,913件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

PEMicro is responsible for their scripts and SW for programming/debugging. Other than the S32DS IDE debug scripts, I am not familiar with other alternatives.

Debuggers such as J-Link (SEGGER) provides the J-FLASH software which is free of charge.

Best regards,
Julián

0 件の賞賛
返信