[S32 SDK for S32K344] Cannot Open BMS Example Config MEX file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32 SDK for S32K344] Cannot Open BMS Example Config MEX file

跳至解决方案
2,932 次查看
richespiritu
Contributor II

I've been having trouble opening the .mex file of the HVBMS bringup project. I've tried a couple of reinstalls but I always run into this error when opening the configuration file. Here is my installation details.

Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.3; Build id: 202306291736
Package: S32K3 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Package: SW32K3 BMS SDK Autosar 4.4 R21-11 Version 1.0.2; Version: 1.0.2; Build id: 202402061436
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.5.7; Build id: 202304031909
Package: S32K3xx development package; Version: 3.5.0 RTM; Build id: 202304051438
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202109281337
Package: S32 Design Studio Platform Tools package; Version: 3.5.3; Build id: 202306291736
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: SW32K3 BMS SL SDK Autosar 4.4 R21-11 Version 1.0.2 DEMO; Version: 1.0.2; Build id: 202402061316

richespiritu_0-1709086945454.png

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,921 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you forget install S32K3xx development package 3.5.2.202304051438. Please refer to the step 3 of HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

6 回复数
2,903 次查看
richespiritu
Contributor II

I have since updated most of the packages to the latest version, but it still would not let me open the configuration files (.mex).

I have also tried opening examples, so that I am opening it from "C:\Users\rich_\workspaceS32DS.3.5\" directory, since I saw that as a potential problem for others. Please advice, thanks. Here is my updated installation information:

Package: S32 Design Studio Platform package; Version: 3.5.10; Build id: 202401301332
Package: S32K3 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Package: S32K3xx development package; Version: 3.5.8; Build id: 202311290134
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202307190908
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: S32K3XX.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 HF01; Version: 4.0.0; Build id: 202401161212
Package: GDB Client for Arm Embedded Processors 12.1 Build 1702; Version: 1702; Build id: 202309251304
Package: S32K3.P01 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202304031555
Package: CANTRCV_TJA1145A for S32K3; Version: 0.8.0; Build id: 202305240834
Package: SW32K3 BMS SDK Autosar 4.4 R21-11 Version 1.0.2; Version: 1.0.2; Build id: 202402061436
Package: FS26 for S32K3 version 2.0.0; Version: 2.0.0; Build id: 202308040805
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202307190917
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.7.6; Build id: 202312041432
Package: S32 Design Studio Platform Tools package; Version: 3.5.10; Build id: 202401301332
Package: SW32K3 BMS SL SDK Autosar 4.4 R21-11 Version 1.0.2 DEMO; Version: 1.0.2; Build id: 202402061316
Package: S32 Design Studio Debugger Core; Version: 3.5.10; Build id: 202401301027

0 项奖励
回复
2,890 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I only installed S32K3 RTD 3.0.0 completely according to "HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5" and did not encounter this problem.
I am able to open .mex file of HvBms400_774_722_TPL_Bring_Up even if HVBMS related software is not installed.
So I later did not install these software according to SW32K344_HVBMS-RD_Bring-up_Example_S32DS_1_0_2_ReleaseNotes.txt.

S32K3xx development package 3.5.2.202304051438.png

0 项奖励
回复
2,888 次查看
richespiritu
Contributor II

Hi Robin,

I uninstalled and reinstalled RTD 3.0.0 based on the instructions, and I was eventually able to open it. My problem now is that going through the tabs in the configurator tool is super slow. When opening the .mex file on startup takes 10 minutes, and s32 design studio enters a (not responsive) state.

0 项奖励
回复
2,885 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Similar issues have been discussed in this post: S32DS Config Tool Extremely Slow with S32K3 HVBMS. It is recommended that you ask our S32DS experts.

0 项奖励
回复
2,908 次查看
richespiritu
Contributor II

Hi

I believe I already have it installed, as seen in the installation information above. i have tried opening a different project, the bring-up example for MC33775, and this is the message that I get.

richespiritu_0-1709146286548.png

 

0 项奖励
回复
2,922 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Seems that you forget install S32K3xx development package 3.5.2.202304051438. Please refer to the step 3 of HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------