LPUART Example code not working with eDMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPUART Example code not working with eDMA

ソリューションへジャンプ
7,186件の閲覧回数
axb
Contributor II

Project is created from S32K144 EAR SDK Example Projects. But there is no communication with UART. The same code is working with Interrupts. I have changed lpuart_user_config_t lpuart1_InitConfig0. (.transferType = LPUART_USING_DMA,)

Am I missing any configuration?

1 解決策
6,572件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

to be able use  eDMA  data transfer mode - you also need init eDMA driver by adding this line in the main function:

EDMA_DRV_Init(&dmaController1_State, &dmaController1_InitConfig0);

front of UART init. 

Another suggestion from SDK team is to use latest RTM SDK version. Lot of bugs is fixed there. 

Jiri 

元の投稿で解決策を見る

6 返答(返信)
6,573件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

to be able use  eDMA  data transfer mode - you also need init eDMA driver by adding this line in the main function:

EDMA_DRV_Init(&dmaController1_State, &dmaController1_InitConfig0);

front of UART init. 

Another suggestion from SDK team is to use latest RTM SDK version. Lot of bugs is fixed there. 

Jiri 

6,572件の閲覧回数
axb
Contributor II

Thanks. It worked. Could you let me know how do I update my current SDK?

0 件の賞賛
返信
6,572件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

If you have installed all updates (main menu bar -> Help -> Check for updates) - you can create project from example with latest SDK version 

pastedImage_1.png

Jiri

6,572件の閲覧回数
axb
Contributor II

Could you also look into another question of mine https://community.nxp.com/thread/456468?sr=inbox ?

0 件の賞賛
返信
6,572件の閲覧回数
axb
Contributor II

Thanks

0 件の賞賛
返信
6,572件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

I tried LPUART example - and for me even the interrupt mode is not working correctly. I can get welcome message, but no response to typing. I sent email to SDK team for solution and I'll respond when I get answer. 

Jiri