[LIN Stack] Error bit is set master node sends only header but no data bytes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[LIN Stack] Error bit is set master node sends only header but no data bytes

1,619 次查看
SorinT
Contributor I

Hello,

I am having an issue with the LIN Stack from the S32SDK RTM 4.0.2.

I am using the S32K144 uC, configured as LIN slave.

It seems that when the master node sends a frame header but without any data bytes (frame is supposed to be published by master), our LIN stack sets the error bit when it shouldnt.

According to the LIN specifications (LIN 2.1 Specifications chapter 2.7.4), the error bit should be set when there are errors in the response field, but should not be set when there is no response at all.

Could you please support me in finding the root cause? Maybe I am missing somethinh?

 

Best Regards,

Sorin

 

标签 (1)
0 项奖励
回复
1 回复

1,611 次查看
PetrS
NXP TechSupport
NXP TechSupport
0 项奖励
回复