Build version difference

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build version difference

1,598 次查看
jetty1012
Contributor II

Hi,

I'm using S32 DS to generate some driver code, and I found many files(generated by other people) that I didn't modify also changed. And the only difference is the build version.

We're using the same DS and SDK, why are the build versions different?

jetty1012_0-1686208661992.png

Thanks,

Jetty

标签 (1)
0 项奖励
回复
2 回复数

1,534 次查看
NamLee
NXP Employee
NXP Employee

Hi jetty1012,

Due to it's only the fixed comment parts in the package, so i think that the package RTD in other's PC is not the same. We have the RTD 3.0.0 release and RTD 3.0.0 P01.

K3_3.0.0 and 3.0.0 P01.png

Could you please help me to check the version of RTD package installed in the PC?

Please let me know if you have any further information.

Thank you,

Nam.

0 项奖励
回复

1,558 次查看
jetty_1012
Contributor II

It seems to be a hard question..

0 项奖励
回复