Build version difference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build version difference

1,954件の閲覧回数
jetty1012
Contributor II

Hi,

I'm using S32 DS to generate some driver code, and I found many files(generated by other people) that I didn't modify also changed. And the only difference is the build version.

We're using the same DS and SDK, why are the build versions different?

jetty1012_0-1686208661992.png

Thanks,

Jetty

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,890件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi jetty1012,

Due to it's only the fixed comment parts in the package, so i think that the package RTD in other's PC is not the same. We have the RTD 3.0.0 release and RTD 3.0.0 P01.

K3_3.0.0 and 3.0.0 P01.png

Could you please help me to check the version of RTD package installed in the PC?

Please let me know if you have any further information.

Thank you,

Nam.

0 件の賞賛
返信

1,914件の閲覧回数
jetty_1012
Contributor II

It seems to be a hard question..

0 件の賞賛
返信