Build version difference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build version difference

1,954 Views
jetty1012
Contributor II

Hi,

I'm using S32 DS to generate some driver code, and I found many files(generated by other people) that I didn't modify also changed. And the only difference is the build version.

We're using the same DS and SDK, why are the build versions different?

jetty1012_0-1686208661992.png

Thanks,

Jetty

Labels (1)
0 Kudos
Reply
2 Replies

1,890 Views
NamLee
NXP Employee
NXP Employee

Hi jetty1012,

Due to it's only the fixed comment parts in the package, so i think that the package RTD in other's PC is not the same. We have the RTD 3.0.0 release and RTD 3.0.0 P01.

K3_3.0.0 and 3.0.0 P01.png

Could you please help me to check the version of RTD package installed in the PC?

Please let me know if you have any further information.

Thank you,

Nam.

0 Kudos
Reply

1,914 Views
jetty_1012
Contributor II

It seems to be a hard question..

0 Kudos
Reply