whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

跳至解决方案
2,322 次查看
jinshuaixu
Contributor V

hello, friends

        l can use "codewarrior IDE" generate '.abs' file ago, now l use s32ds software , l want generate '.abs' file , how to set s32ds software?

        the reason that l want to get '.abs' file is that l want use "vector ASAP2 edit" software to monitor address and variable data.

     thank you.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,160 次查看
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,161 次查看
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

0 项奖励
回复
2,160 次查看
jinshuaixu
Contributor V

Hi

     Thank you for you response.May you good luck.

0 项奖励
回复