whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

ソリューションへジャンプ
1,343件の閲覧回数
jinshuaixu
Contributor V

hello, friends

        l can use "codewarrior IDE" generate '.abs' file ago, now l use s32ds software , l want generate '.abs' file , how to set s32ds software?

        the reason that l want to get '.abs' file is that l want use "vector ASAP2 edit" software to monitor address and variable data.

     thank you.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,181件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,182件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

0 件の賞賛
返信
1,181件の閲覧回数
jinshuaixu
Contributor V

Hi

     Thank you for you response.May you good luck.

0 件の賞賛
返信