s32ds 3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,853件の閲覧回数
Anjalipurushothaman
Contributor III

Please find attached While debugging, port is not showing up in the window. Checked the com port the board is getting detected , but in the debug configuration tab it is not showing

0 件の賞賛
返信
1 解決策
6,807件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

 

As I see Debug option is available, please can you give a shot and hit Debug button whether it is working or not, and if follows up with any error message please can you reply with the particular error message. 

Mehul_Patel_NXP_0-1685532269547.png

Thank you. Best regards.

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,793件の閲覧回数
Anjalipurushothaman
Contributor III
 
0 件の賞賛
返信
6,798件の閲覧回数
Anjalipurushothaman
Contributor III

please find the error iam getting

0 件の賞賛
返信
6,766件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

Please can you check that required driver is installed properly? 

You can download relevant driver as per your system configurations from:  https://ftdichip.com/drivers/

Please can you try it and revert whether it is working or not. 

Thank you. Best regards. 

- Mehul

0 件の賞賛
返信
6,738件の閲覧回数
Anjalipurushothaman
Contributor III

Thanks for your reply,Still the same error.

Please provide the link of required drivers for S32K3X8EVB-Q289 evaluation board on s32DS 3.5.

0 件の賞賛
返信
6,808件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

 

As I see Debug option is available, please can you give a shot and hit Debug button whether it is working or not, and if follows up with any error message please can you reply with the particular error message. 

Mehul_Patel_NXP_0-1685532269547.png

Thank you. Best regards.

 

0 件の賞賛
返信