s32ds 3.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32ds 3.5

Jump to solution
6,859 Views
Anjalipurushothaman
Contributor III

Please find attached While debugging, port is not showing up in the window. Checked the com port the board is getting detected , but in the debug configuration tab it is not showing

0 Kudos
Reply
1 Solution
6,813 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

 

As I see Debug option is available, please can you give a shot and hit Debug button whether it is working or not, and if follows up with any error message please can you reply with the particular error message. 

Mehul_Patel_NXP_0-1685532269547.png

Thank you. Best regards.

 

View solution in original post

0 Kudos
Reply
5 Replies
6,799 Views
Anjalipurushothaman
Contributor III
 
0 Kudos
Reply
6,804 Views
Anjalipurushothaman
Contributor III

please find the error iam getting

0 Kudos
Reply
6,772 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

Please can you check that required driver is installed properly? 

You can download relevant driver as per your system configurations from:  https://ftdichip.com/drivers/

Please can you try it and revert whether it is working or not. 

Thank you. Best regards. 

- Mehul

0 Kudos
Reply
6,744 Views
Anjalipurushothaman
Contributor III

Thanks for your reply,Still the same error.

Please provide the link of required drivers for S32K3X8EVB-Q289 evaluation board on s32DS 3.5.

0 Kudos
Reply
6,814 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Anjalipurushothaman ,

 

As I see Debug option is available, please can you give a shot and hit Debug button whether it is working or not, and if follows up with any error message please can you reply with the particular error message. 

Mehul_Patel_NXP_0-1685532269547.png

Thank you. Best regards.

 

0 Kudos
Reply