procesor expert looks disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

procesor expert looks disable

跳至解决方案
4,517 次查看
albertgalofre
Contributor II

Hi there,
I have installed recently the S32DS IDE.
After open a S32DS example ("\workspaceS32DS.ARM.2.2\hello_world_s32k118"); the hieratically file structure appears with several items with its own icon, with a line in the middle. They seem disable; nevertheless, I can open them and edit.
I have generated the code from processorexpert; and compile and seems works fine.

 

Beore to start to develope my firmware I MUST to assert that there is no problem with these items/icons.

Attach a picture where you can see what I am speaking about.
Thanks a lot

 

 

0 项奖励
回复
1 解答
4,503 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, if code generator works - there is no issue. This is just way how Eclipse shows files excluded from build itself. 

在原帖中查看解决方案

3 回复数
4,505 次查看
albertgalofre
Contributor II

Hi Jiri,

Thanks for your quick answer.

So I assume, that in the same way, there is NO PROBLEM with the ProcessorExpert.pe file. I'm right?

 

thanks in advance

0 项奖励
回复
4,504 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, if code generator works - there is no issue. This is just way how Eclipse shows files excluded from build itself. 

4,509 次查看
jiri_kral
NXP Employee
NXP Employee

Hi,

files with gray color are excluded from build - typically documentation, config files and so on. This Eclipse feature does not  affect build itself. 

 

Jiri 

0 项奖励
回复