procesor expert looks disable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

procesor expert looks disable

ソリューションへジャンプ
4,509件の閲覧回数
albertgalofre
Contributor II

Hi there,
I have installed recently the S32DS IDE.
After open a S32DS example ("\workspaceS32DS.ARM.2.2\hello_world_s32k118"); the hieratically file structure appears with several items with its own icon, with a line in the middle. They seem disable; nevertheless, I can open them and edit.
I have generated the code from processorexpert; and compile and seems works fine.

 

Beore to start to develope my firmware I MUST to assert that there is no problem with these items/icons.

Attach a picture where you can see what I am speaking about.
Thanks a lot

 

 

0 件の賞賛
返信
1 解決策
4,495件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, if code generator works - there is no issue. This is just way how Eclipse shows files excluded from build itself. 

元の投稿で解決策を見る

3 返答(返信)
4,497件の閲覧回数
albertgalofre
Contributor II

Hi Jiri,

Thanks for your quick answer.

So I assume, that in the same way, there is NO PROBLEM with the ProcessorExpert.pe file. I'm right?

 

thanks in advance

0 件の賞賛
返信
4,496件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, if code generator works - there is no issue. This is just way how Eclipse shows files excluded from build itself. 

4,501件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

files with gray color are excluded from build - typically documentation, config files and so on. This Eclipse feature does not  affect build itself. 

 

Jiri 

0 件の賞賛
返信