mpc5777c 516 uart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5777c 516 uart

Jump to solution
3,563 Views
saichinnala
Contributor II

i am using mpc5777c eval board on that i am trying uart s32ds example code but am unable to get communication successfully

i had a doubt that in transmitting part that there is code related to pointing data to sdr register

@lukaszadrapa 

Tags (1)
0 Kudos
Reply
1 Solution
3,514 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the SDK example "esci_transfer_mpc5777c" is setting module to RX loopback mode, so MCU's RXD pin is disconnected from eSCI module, however you should be able to see transmitted data, if looking on right TXD pin (GPIO83, AE19). 
You can modify the eSCI setting in component to use dual wire mode.

BR, Petr

 

View solution in original post

0 Kudos
Reply
2 Replies
3,515 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the SDK example "esci_transfer_mpc5777c" is setting module to RX loopback mode, so MCU's RXD pin is disconnected from eSCI module, however you should be able to see transmitted data, if looking on right TXD pin (GPIO83, AE19). 
You can modify the eSCI setting in component to use dual wire mode.

BR, Petr

 

0 Kudos
Reply
3,490 Views
saichinnala
Contributor II

i used uart sdk example code but i am unable to communicate on terminal,can you please help me here 

0 Kudos
Reply