mpc5777c 516 uart

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mpc5777c 516 uart

跳至解决方案
3,544 次查看
saichinnala
Contributor II

i am using mpc5777c eval board on that i am trying uart s32ds example code but am unable to get communication successfully

i had a doubt that in transmitting part that there is code related to pointing data to sdr register

@lukaszadrapa 

标记 (1)
0 项奖励
回复
1 解答
3,495 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the SDK example "esci_transfer_mpc5777c" is setting module to RX loopback mode, so MCU's RXD pin is disconnected from eSCI module, however you should be able to see transmitted data, if looking on right TXD pin (GPIO83, AE19). 
You can modify the eSCI setting in component to use dual wire mode.

BR, Petr

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,496 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the SDK example "esci_transfer_mpc5777c" is setting module to RX loopback mode, so MCU's RXD pin is disconnected from eSCI module, however you should be able to see transmitted data, if looking on right TXD pin (GPIO83, AE19). 
You can modify the eSCI setting in component to use dual wire mode.

BR, Petr

 

0 项奖励
回复
3,471 次查看
saichinnala
Contributor II

i used uart sdk example code but i am unable to communicate on terminal,can you please help me here 

0 项奖励
回复