is it possible to change S32DS generated code directory?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

is it possible to change S32DS generated code directory?

2,464 次查看
babytiger
Contributor II

When the code is generated from a *.mex file, "RTD", "board", and "generate" folders are created.
Is it possible to change S32DS generated code/folder path?


■ S32DS version:
S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 1)

0 项奖励
回复
1 回复

2,436 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

You cannot change the location of the generated code, but you can export the source files to any location you wish.

Use the right click -> Export option to bring up the tool:

mikedoidge_0-1640022300952.png

Under 'S32 Configuration Tools', select the 'Export Source Files' option for the tool you wish (only Pins, Clocks, and Peripherals supported for this).

mikedoidge_1-1640023048600.png

Now you can specify any location you want.

Best regards,

Mike

0 项奖励
回复