is it possible to change S32DS generated code directory?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is it possible to change S32DS generated code directory?

2,456 Views
babytiger
Contributor II

When the code is generated from a *.mex file, "RTD", "board", and "generate" folders are created.
Is it possible to change S32DS generated code/folder path?


■ S32DS version:
S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 1)

0 Kudos
Reply
1 Reply

2,428 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

You cannot change the location of the generated code, but you can export the source files to any location you wish.

Use the right click -> Export option to bring up the tool:

mikedoidge_0-1640022300952.png

Under 'S32 Configuration Tools', select the 'Export Source Files' option for the tool you wish (only Pins, Clocks, and Peripherals supported for this).

mikedoidge_1-1640023048600.png

Now you can specify any location you want.

Best regards,

Mike

0 Kudos
Reply