is it possible to change S32DS generated code directory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is it possible to change S32DS generated code directory?

1,704件の閲覧回数
babytiger
Contributor II

When the code is generated from a *.mex file, "RTD", "board", and "generate" folders are created.
Is it possible to change S32DS generated code/folder path?


■ S32DS version:
S32 Design Studio for S32 Platform
Version: 3.4
Build id: 201217 (Update 1)

0 件の賞賛
返信
1 返信

1,676件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

You cannot change the location of the generated code, but you can export the source files to any location you wish.

Use the right click -> Export option to bring up the tool:

mikedoidge_0-1640022300952.png

Under 'S32 Configuration Tools', select the 'Export Source Files' option for the tool you wish (only Pins, Clocks, and Peripherals supported for this).

mikedoidge_1-1640023048600.png

Now you can specify any location you want.

Best regards,

Mike

0 件の賞賛
返信