enabling S32K146 floating point instructions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enabling S32K146 floating point instructions

ソリューションへジャンプ
3,779件の閲覧回数
KelvinSmith
Contributor III

The S32K146 processor includes a floating point unit, but if I go into the project properties and under 'target processor', I set 'Float ABI' to 'FP instructions (hard)', I get errors during the link stage like these:

c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: error: libuavcanV1_demo.elf uses VFP register arguments, ./Project_Settings/Startup_Code/system_S32K146.o does not
c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: failed to merge target specific data of file ./Project_Settings/Startup_Code/system_S32K146.o

These errors repeat for every source file, even if they do not use floating point instructions.

0 件の賞賛
返信
1 解決策
3,727件の閲覧回数
KelvinSmith
Contributor III

I solved this by doing a clean on the project. That caused a bunch of new errors. So I deleted the project from the workspace and readded it. Then I built it again and presto it worked! What a lot of nonesense. But at least it is possible.

元の投稿で解決策を見る

4 返答(返信)
3,747件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Do you have chosen right FPU type (FPv4-SP)?

0 件の賞賛
返信
3,729件の閲覧回数
KelvinSmith
Contributor III

The only option is fpv4-sp-d16, forcibly selected. Presumably this is the same as fpv4-sp

0 件の賞賛
返信
3,749件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this typically happen if you are linking external library which is compiled with soft FP. It is possible share your project? 

3,728件の閲覧回数
KelvinSmith
Contributor III

I solved this by doing a clean on the project. That caused a bunch of new errors. So I deleted the project from the workspace and readded it. Then I built it again and presto it worked! What a lot of nonesense. But at least it is possible.