enabling S32K146 floating point instructions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

enabling S32K146 floating point instructions

跳至解决方案
3,753 次查看
KelvinSmith
Contributor III

The S32K146 processor includes a floating point unit, but if I go into the project properties and under 'target processor', I set 'Float ABI' to 'FP instructions (hard)', I get errors during the link stage like these:

c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: error: libuavcanV1_demo.elf uses VFP register arguments, ./Project_Settings/Startup_Code/system_S32K146.o does not
c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: failed to merge target specific data of file ./Project_Settings/Startup_Code/system_S32K146.o

These errors repeat for every source file, even if they do not use floating point instructions.

0 项奖励
回复
1 解答
3,701 次查看
KelvinSmith
Contributor III

I solved this by doing a clean on the project. That caused a bunch of new errors. So I deleted the project from the workspace and readded it. Then I built it again and presto it worked! What a lot of nonesense. But at least it is possible.

在原帖中查看解决方案

4 回复数
3,721 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Do you have chosen right FPU type (FPv4-SP)?

0 项奖励
回复
3,703 次查看
KelvinSmith
Contributor III

The only option is fpv4-sp-d16, forcibly selected. Presumably this is the same as fpv4-sp

0 项奖励
回复
3,723 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this typically happen if you are linking external library which is compiled with soft FP. It is possible share your project? 

3,702 次查看
KelvinSmith
Contributor III

I solved this by doing a clean on the project. That caused a bunch of new errors. So I deleted the project from the workspace and readded it. Then I built it again and presto it worked! What a lot of nonesense. But at least it is possible.