When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

1,852件の閲覧回数
DiZhang
NXP Employee
NXP Employee

DiZhang_0-1660113542528.png

as the picture show:

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://www.pemicro.com/eclipse/updates/com.pemicro.debug.gdbjtag.pne.updatesite/5.2.6/plugins/com.pe....
Read timed out

0 件の賞賛
返信
3 返答(返信)

1,845件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @DiZhang,

Can you retry after deleting S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.core\cache\ and S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.repository\cache\?

Best Regards,

Mike

0 件の賞賛
返信

1,842件の閲覧回数
DiZhang
NXP Employee
NXP Employee

Thank you for your reply. I had solved this problem yet.

I think the reason is that the install sequence of update package is not right.

0 件の賞賛
返信

1,837件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

@DiZhang,

It's possible your installation is missing a required update to the P&E drivers. Please go to Help -> Install New Software and then select 'PEMicro - http://www.pemicro.com/eclipse/updates' to check that you have the latest updates and get them installed, next check that you have the S32K3 Development Package, and then try the S32K3 RTD install again.

Best Regards,

Mike

0 件の賞賛
返信