When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When installing SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204, several errors occurred as follow

1,673 Views
DiZhang
NXP Employee
NXP Employee

DiZhang_0-1660113542528.png

as the picture show:

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://www.pemicro.com/eclipse/updates/com.pemicro.debug.gdbjtag.pne.updatesite/5.2.6/plugins/com.pe....
Read timed out

0 Kudos
Reply
3 Replies

1,666 Views
mikedoidge
NXP Employee
NXP Employee

Hello @DiZhang,

Can you retry after deleting S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.core\cache\ and S32DS.3.4\eclipse\p2\org.eclipse.equinox.p2.repository\cache\?

Best Regards,

Mike

0 Kudos
Reply

1,663 Views
DiZhang
NXP Employee
NXP Employee

Thank you for your reply. I had solved this problem yet.

I think the reason is that the install sequence of update package is not right.

0 Kudos
Reply

1,658 Views
mikedoidge
NXP Employee
NXP Employee

@DiZhang,

It's possible your installation is missing a required update to the P&E drivers. Please go to Help -> Install New Software and then select 'PEMicro - http://www.pemicro.com/eclipse/updates' to check that you have the latest updates and get them installed, next check that you have the S32K3 Development Package, and then try the S32K3 RTD install again.

Best Regards,

Mike

0 Kudos
Reply