When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support

1,850件の閲覧回数
justforfunl
Contributor II

The function is not implemented. Rebuild the library with Windows, GTK+ 2.x or Carbon support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script.

Question 1: is the S32 Design Vision Studio's ocv library compiled with GTK2.0?

Question 2: How to compile the GTK for s32v234 kernel.

Question 3: How to compile OpenCV With GTK2.0 for Arm or with QT.

ラベル(2)
タグ(4)
0 件の賞賛
返信
0 返答(返信)