When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support

1,923 次查看
justforfunl
Contributor II

The function is not implemented. Rebuild the library with Windows, GTK+ 2.x or Carbon support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script.

Question 1: is the S32 Design Vision Studio's ocv library compiled with GTK2.0?

Question 2: How to compile the GTK for s32v234 kernel.

Question 3: How to compile OpenCV With GTK2.0 for Arm or with QT.

标签 (2)
标记 (4)
0 项奖励
回复
0 回复数