Unable to Add Component in S32DS ARM 2.2, menu option disabled, "Predecessor Expert" not working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Add Component in S32DS ARM 2.2, menu option disabled, "Predecessor Expert" not working?

ソリューションへジャンプ
3,722件の閲覧回数
rsating
Contributor III

I'm working through the following BCC example for S32K144-EVB

Battery Cell Controller (BCC) software driver for MC33771C
Sec 4.4 Creating a new project with BCC SW driver
https://www.nxp.com/docs/en/user-guide/UM11346.pdf

However, I'm not able to get "Processor Expert" functionality to work.

Trying to add the "lpspi" component to the project, the context menu option is disabled, see below, and there are not "Components" nodes on the tree in Project Explorer as there are in S32S for ARM 2.0:

BCC_S32K144_Component_AddToProject.png

All S32DS updates are applied, and all available S32 Design Studio components are installed:

BCC_S32K144_ARM-2.2_AvailableSoftware.png

What could I be missing, that components can't be added to the project?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,684件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rsating,

 

How about create a simple new project ?

I test on my side, it seems can work:

Alice_Yang_0-1606286002192.png

 

 

Regards,

Alice

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,685件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rsating,

 

How about create a simple new project ?

I test on my side, it seems can work:

Alice_Yang_0-1606286002192.png

 

 

Regards,

Alice

 

0 件の賞賛
返信
3,676件の閲覧回数
rsating
Contributor III

I was able to see the Components Library in a new project, but only after noticing and clicking on the "Components Library" tab to make it visible.  Until then, the menu option  Window --> Show View --> Components  appears to not do anything. One has to look carefully, it the tab was there, but not easy to see. I suggest making the tab active after the user tries to make it visible with using the menu click sequence below, otherwise, it is hard to understand what, if anything, happened. 

S32DS_showing-components-library.png

0 件の賞賛
返信