Unable to Add Component in S32DS ARM 2.2, menu option disabled, "Predecessor Expert" not working?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to Add Component in S32DS ARM 2.2, menu option disabled, "Predecessor Expert" not working?

跳至解决方案
3,778 次查看
rsating
Contributor III

I'm working through the following BCC example for S32K144-EVB

Battery Cell Controller (BCC) software driver for MC33771C
Sec 4.4 Creating a new project with BCC SW driver
https://www.nxp.com/docs/en/user-guide/UM11346.pdf

However, I'm not able to get "Processor Expert" functionality to work.

Trying to add the "lpspi" component to the project, the context menu option is disabled, see below, and there are not "Components" nodes on the tree in Project Explorer as there are in S32S for ARM 2.0:

BCC_S32K144_Component_AddToProject.png

All S32DS updates are applied, and all available S32 Design Studio components are installed:

BCC_S32K144_ARM-2.2_AvailableSoftware.png

What could I be missing, that components can't be added to the project?

Thanks

0 项奖励
回复
1 解答
3,740 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rsating,

 

How about create a simple new project ?

I test on my side, it seems can work:

Alice_Yang_0-1606286002192.png

 

 

Regards,

Alice

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,741 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rsating,

 

How about create a simple new project ?

I test on my side, it seems can work:

Alice_Yang_0-1606286002192.png

 

 

Regards,

Alice

 

0 项奖励
回复
3,732 次查看
rsating
Contributor III

I was able to see the Components Library in a new project, but only after noticing and clicking on the "Components Library" tab to make it visible.  Until then, the menu option  Window --> Show View --> Components  appears to not do anything. One has to look carefully, it the tab was there, but not easy to see. I suggest making the tab active after the user tries to make it visible with using the menu click sequence below, otherwise, it is hard to understand what, if anything, happened. 

S32DS_showing-components-library.png

0 项奖励
回复