Processor Expert Component Inspector view is blank, Components View cannot be shown

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Component Inspector view is blank, Components View cannot be shown

ソリューションへジャンプ
2,661件の閲覧回数
rsating
Contributor III

The Processor Expert "Components Inspector" view is blank for my project, see screenshot below. Also, the "Components" view refuses to display.  Could it be due to the "Peripheral is already used" error?

S32DS_component-inspector-empty.png

Below is the menu sequence used in attempting to display the "Components" view:

S32DS_show-view_components.png

Why does the view not open?  How can we troubleshoot the errors without it?  I may have added components more than once, but I cannot see a way to investigate or resolve the problem. Can you help us understand how this works?

Attached is the S32DS project, in case it helps.

Thanks

0 件の賞賛
返信
1 解決策
2,649件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this example is for older SDK version which is not supported by S32DS for ARN v2.2. Try to open it with S32DS for ARM 2018.R1

 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,649件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this example is for older SDK version which is not supported by S32DS for ARN v2.2. Try to open it with S32DS for ARM 2018.R1

 

Jiri 

0 件の賞賛
返信