Turn on the "Path, Location of error " in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Turn on the "Path, Location of error " in S32DS

Jump to solution
1,730 Views
tuanhoc8
Contributor II

 

Hello everyone, I have a problem and need help:
I lost Location and Path of error when building project. How to turn on it?

I'll appreciate any help.

Cheers,

Tuan.

0 Kudos
Reply
1 Solution
1,651 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

you are probably mixing two Autosar versions as is written in the first #error message. It is possible share your project? 

 

View solution in original post

0 Kudos
Reply
5 Replies
1,704 Views
tuanhoc8
Contributor II

@jiri_kral

 This is my "Problem view". when i double click on the error, I can't go to the error line. However, on the S32DS of my friend, the double will bring to the line of the error. 

tuanhoc8_0-1698858786437.png

 

0 Kudos
Reply
1,652 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

you are probably mixing two Autosar versions as is written in the first #error message. It is possible share your project? 

 

0 Kudos
Reply
1,574 Views
tuanhoc8
Contributor II

@jiri_kral Sorry, I have just recieved a message from Gmail today.
Tks you again for taking a time for my project. I have fixed it tks you too much

1,709 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share the output from build console? 

0 Kudos
Reply
1,692 Views
tuanhoc8
Contributor II

@jiri_kral 

This is the "Problem view" of my friend.

 

tuanhoc8_0-1698889996415.png

After build the path and location of error  appear and he just click on it, the line of the error is selected. However, my S32DS doesn't have the path and location of error after build.

0 Kudos
Reply