To build and run the IPCF Sample program (S32 IPCF 1.1.0 D2012) on S32DS (Ver: 3.3,Build id: 2006)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To build and run the IPCF Sample program (S32 IPCF 1.1.0 D2012) on S32DS (Ver: 3.3,Build id: 2006)

8,702件の閲覧回数
_manoj_kumar
NXP Employee
NXP Employee

Hello Team,

Customer facing below errors in S32 DS 3.3, pls advice:

    • Error: Processor 'S32G274A' detected in Design Studio GCC project does not match with currently selected `S32G274A_Rev2`.
    • Level: Error
    • Type: Tool problem
    • Tool: McuConfiguration
    • Origin: IPCF_Example_S32G274
    • Resource: Processor
    • Information: -
  • If they switch to S32G274A, then there are attached build errors

Please find more details.

Design Studio : Version: 3.3,Build id: 200610

RTD Version : SW32G2_RTD_4.4_0.9.0

IPCF Sample program (S32 IPCF 1.1.0 D2012

Documents Referred: IPCF Shared Memory Driver User Manual Version 1.4

They are observing issues in S32 Design Studio. They are unable to select appropriate hardware to configure.

Once the IPCF example project is imported in DS, there is a mismatch BGA observed.

_manoj_kumar_0-1614594447759.jpeg

Even if they choose S32G2745A_525bga the tool does not support selected processor.

_manoj_kumar_1-1614594447728.jpeg

Please let me know if you need any other details to be checked with them

Thanks

0 件の賞賛
返信
4 返答(返信)

8,643件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @_manoj_kumar ,

It's possible some package or update is not installed. Could you please go to S32DS Extensions and Updates menu and click on 'Installation Details' link at upper right. Then send the details of the installed packages.

mikedoidge_0-1615501520413.png

 

Thanks,

Mike

0 件の賞賛
返信

8,617件の閲覧回数
_manoj_kumar
NXP Employee
NXP Employee

Hello Mr. Mike,

The solution for this issue was provided. Please find the link below.

https://community.nxp.com/t5/Vehicle-Control-and-Networking/To-build-and-run-the-IPCF-Sample-program...

Thanks.

8,694件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please attach pictures with higher resolution. Attached ones are too small and unreadable. Thanks. 

 

Jiri 

0 件の賞賛
返信

8,678件の閲覧回数
_manoj_kumar
NXP Employee
NXP Employee

Hi,

I have attached the error snapshots. Please let me know if you need any other details.

Thanks.

0 件の賞賛
返信