DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

1,767件の閲覧回数
lubo_NEW
Contributor III

In S32DS project, you want to set the input/output configuration of GPIO, etc., but the Pin Library Settings are not available As is shown inQQ图片20210303091646.png

0 件の賞賛
返信
2 返答(返信)

1,723件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @lubo_NEW ,

One way to make the view appear, select Hide Views from the Processor Expert menu, then Show Views. It should reopen the views for you. Otherwise you can manually add them from Window -> Show View -> Processor Expert.

image.png

mikedoidge_0-1615500049700.png

Hope it helps,

Mike

0 件の賞賛
返信

1,765件の閲覧回数
lubo_NEW
Contributor III

But the official instructions are shown in the figure for configuring pinsQQ图片20210303091537.png

0 件の賞賛
返信